AXIS#.SAFEPARAM.ABSOLUTEPOSRESETVALUE

Description

Indicates the safe homing position. This is only usable when a safe encoder is configured in the safety parameters and when the absolute position support is enabled (see AXIS#.SAFEPARAM.ABSOLUTEPOSEN). This value must be within the range defined by the encoder multi-turn bits and the parameter AXIS#.SAFEPARAM.ABSOLUTEPOSRANGE. The value must be entered in user units.

Parameters Editor with the Absolute Position Range value circled

Context

For safe encoder details refer to Motor feedback requirements.

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

User units defined in the safety parameters

Range

Depends on the range and user units
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
AXIS1.SAFEPARAM.ABSOLUTEPOSRESETVALUE

3150h

07h

Signed32

-

-

Read/Write

No

AXIS2.SAFEPARAM.ABSOLUTEPOSRESETVALUE

3250h

07h

Signed32

-

-

Read/Write

No